debugger.Interrupt.DeleteTimer
|
This function deletes the timer interrupt setting. [RH850 Simulator]
[Specification format]
debugger.Interrupt.DeleteTimer()
|
[Argument(s)]
None
[Return value]
If the timer interrupt setting was deleted successfully: True
If there was an error when deleting the timer interrupt setting: False
[Detailed description]
- | This function deletes the timer interrupt setting. |
[Example of use]
>>>debugger.Interrupt.ReferTimer()
None
>>>debugger.Interrupt.SetTimer(1, TimeType.S, True)
True
>>>debugger.Interrupt.ReferTimer()
1Second Periodic
>>>debugger.Interrupt.DeleteTimer()
True
>>>debugger.Interrupt.ReferTimer()
None
|