debugger.Breakpoint.Disable
|
This function disables a break point setting.
[Specification format]
debugger.Breakpoint.Disable(breakNumber = "")
|
[Argument(s)]
|
|
breakNumber
|
Specify the break event number to disable.
|
[Return value]
If a break point setting was disabled successfully: True
If there was an error when disabling a break point setting: False
[Detailed description]
- | This function disables the break event specified by breakNumber. |
- | If breakNumber is not specified, then breaks of all break event numbers will be disabled. |
[Example of use]
>>>debugger.Breakpoint.Enable(1)
True
>>>debugger.Breakpoint.Disable(1)
True
>>>debugger.Breakpoint.Delete(1)
True
>>>
|