debugger.Download.BinaryBank


This function downloads a binary file in memory bank format.

[Specification format]

debugger.Download.BinaryBank(fileName, address, append = False, flashErase = False)

[Argument(s)]

Argument

Description

fileName

Specify a download file.

address

Specify a download start address.

append

Specify whether to make an additional download.

True: Perform additional download.

False: Perform overwrite download (default).

flashErase

Specify whether to initialize a flash memory before download.

True: Initialize a flash memory before download.

False: Do not initialize a flash memory before download (default).

Caution

It is not possible to specify only fileName and address.
When specifying both fileName and address, also specify append or both append and flashErase.

[Return value]

If a binary file was downloaded successfully: True

If there was an error when downloading a binary file: False

[Detailed description]

-

When using the memory bank, this function downloads binary files in memory bank format.

[Example of use]

>>>debugger.Download.BinaryBank("C:/test/testModule.bin",  0x1000, False)
True
>>>debugger.Download.BinaryBank("C:/test/testModule2.bin", 0x2000, True)
False
>>>