debugger.Map.Set


This function configures memory mapping.

[Specification format]

debugger.Map.Set(mapType, address1, address2, accessSize = 8, cs = "")

[Argument(s)]

Argument

Description

mapType

Specify a memory type.

The memory types that can be specified are shown below.

Type

Description

MapType.EmulationRom

Emulation ROM area

MapType.EmulationRam

Emulation RAM area

MapType.Target

Target memory area

MapType.TargetRom

Target ROM area

MapType.Stack

Stack area

MapType.Protect

I/O protect area

address1

Specify a map start address.

address2

Specify a map end address.

accessSize

Specify an access size (bit) (default: 8).

For V850, specify either 8, 16, or 32.

For 78K0R [IECUBE], specify either 8 or 16.

cs

Specify the chip select (default: not specified).

When mapping emulation memory (alternative ROM/RAM) in the IECUBE [V850E1], specify the one of the following chip selects as a string: cs0, cs1, cs2, cs3, cs4, cs5, cs6, or cs7.

For models in the V850ES series, however, the chip select allocation is fixed, or the chip select will not function, so this can be omitted.

If chip select is specified, then accessSize cannot be omitted.

[Return value]

If memory mapping was configured successfully: True

If there was an error when configuring memory mapping: False

[Detailed description]

-

This function configures memory mapping with the memory type specified by mapType.

[Example of use]

>>>debugger.Map.Set(MapType.EmulationRom, 0x100000, 0x10ffff)
True
>>>