debugger.XRunBreak.Delete
|
This function deletes XRunBreak information. [V850 Simulator][RH850 Simulator]
[Specification format]
debugger.XRunBreak.Delete()
|
[Argument(s)]
None
[Return value]
If XRunBreak information was deleted successfully: True
If there was an error when deleting XRunBreak information: False
[Detailed description]
- | This function deletes XRunBreak information. |
[Example of use]
>>>debugger.XRunBreak.Refer()
None
>>>debugger.XRunBreak.Set(1, TimeType.S, True)
True
>>>debugger.XRunBreak.Refer()
1Second Periodic
>>>debugger.XRunBreak.Delete()
True
>>>debugger.XRunBreak.Refer()
None
|