debugger.ActionEvent.Delete
|
This function deletes an action event.
[Specification format]
debugger.ActionEvent.Delete(actionEventNumber = "")
|
[Argument(s)]
|
|
actionEventNumber
|
Specify the action event number to delete.
|
[Return value]
If an action event was deleted successfully: True
If there was an error when deleting an action event: False
[Detailed description]
- | This function deletes the action event specified by actionEventNumber. |
- | If actionEventNumber is not specified, then events of all action event numbers will be deleted. |
[Example of use]
>>>debugger.ActionEvent.Delete(1)
True
>>>debugger.ActionEvent.Delete()
True
>>>
|