This function continues program execution.
[Specification format]
debugger.Go(goOption = GoOption.Normal)
|
[Argument(s)]
|
|
goOption
|
Specify an option.
The options that can be specified are shown below.
|
|
|
GoOption.IgnoreBreak
|
Execute ignoring breakpoints.
|
GoOption.WaitBreak
|
Wait until program stops.
|
GoOption.Normal
|
Breakpoints enabled; do not wait until program stops (default).
|
[Return value]
None
[Detailed description]
- | This function continues program execution. |
- | If goOption is specified, the processing is performed in accordance with the specification. |
[Example of use]
>>>debugger.Go()
>>>debugger.Go(GoOption.WaitBreak)
>>>
|