debugger.GetCpuStatus


This function displays the current CPU status.

[Specification format]

debugger.GetCpuStatus()

[Argument(s)]

None

[Return value]

Current CPU status (string)

CPU Status

Description

Hold

In bus hold

HoldStopIdle

Bus hold/Software STOP/Hardware STOP/IDLE mode

PowOff

Power not supplied to the target

InitialStop

Initial stop

Reset

In reset state

Standby

In standby mode

Stop

In STOP mode

StopIdle

Software STOP/Hardware STOP/IDLE mode

Wait

In wait state

Halt

In HALT mode

Sleep

In sleep state

None

N/A

[Detailed description]

-

This function displays the current CPU status.

[Example of use]

>>>debugger.GetCpuStatus()
Stop
>>>