This function clears the coverage memory. [IECUBE][IECUBE2][Simulator]
[Specification format]
debugger.XCoverage.Clear()
|
[Argument(s)]
None
[Return value]
If the coverage memory was cleared successfully: True
If there was an error when clearing the coverage memory: False
[Detailed description]
- | This function clears the coverage memory. |
[Example of use]
>>>debugger.XCoverageClear()
True
>>>
|