This function deletes a conditional timer.
[Specification format]
debugger.Timer.Delete(timerNumber = "")
|
[Argument(s)]
|
|
timerNumber
|
Specify the timer event number to delete.
|
[Return value]
If a timer was deleted successfully: True
If there was an error when deleting a timer: False
[Detailed description]
- | This function deletes the timer of the timer event number specified by timerNumber. |
- | If timerNumber is not specified, then timers of all timer event numbers will be deleted. |
[Example of use]
>>>debugger.Timer.Delete(1)
True
>>>
|