debugger.Upload.Coverage


This function saves the coverage data. [Simulator]

[Specification format]

debugger.Upload.Coverage(fileName, force = False)

[Argument(s)]

Argument

Description

fileName

Specify a file name.

force

Specify whether to overwrite.

True: Overwrite

False: Do not overwrite (default).

[Return value]

If the memory data was uploaded successfully: True

If there was an error when uploading the memory data: False

[Detailed description]

-

This function saves the coverage data to a file.

[Example of use]

>>>debugger.Upload.Coverage("C:/test/coverageData.csrcv")
True
>>>