debugger.GetIORList


This function displays a list of the IORs and SFRs.

[Specification format]

debugger.GetIORList(category = "")

[Argument(s)]

Argument

Description

category

Specify the category in which IORs and SFRs are defined (default: not specified).

[Return value]

List of IOR and SFR information (see the IORInfo class for detail)

[Detailed description]

-

This function displays a list of the IORs and SFRs of the active project.

-

This function displays a list of the IORs and SFRs defined in category.

-

If category is not specified, a list of all IORs and SFRs.

-

This function displays a list of the IORs and SFRs in the following format.

IOR-or-SFR-name value type size address

[Example of use]

>>> ior = debugger.GetIORList()
AD0.ADDRA 0x0000 IOR 2 0x00088040
AD0.ADDRB 0x0000 IOR 2 0x00088042
AD0.ADDRC 0x0000 IOR 2 0x00088044
        :
>>> print ior[0].IORName
AD0.ADDRA
>>> print funcinfo[0].Type
IOR
>>> print funcinfo[0].Address
557120
>>> debugger.GetIORList("DMA0")
DMAC0.DMCSA 0x00000000 IOR 4 0x00082000
        :
DMAC0.DMMOD.SMOD 0x0 IOR 3bits 0x8200c.12
DMAC0.DMMOD.SZSEL 0x0 IOR 3bits 0x8200c.16