debugger.Timer.Disable


This function disables a conditional timer.

[Specification format]

debugger.Timer.Disable(timerNumber = "")

[Argument(s)]

Argument

Description

timerNumber

Specify the timer event number to disable.

[Return value]

If a timer setting was disabled successfully: True

If there was an error when disabling a timer setting: False

[Detailed description]

-

This function disables the timer of the timer event specified by timerNumber.

-

If timerNumber is not specified, then timers of all timer event numbers will be disabled.

[Example of use]

>>>debugger.Timer.Disable(1)
True
>>>