This function evaluates an address expression.
Converted address (numerical value)
If a script is specified to execute in the CubeSuite+.exe startup options, then the symbol conversion function will not be available until the debugging tool is connected. In other words, this function cannot be used, so execute it after connection. |
When a load module name or file name is specified in an address expression, it needs to be enclosed in double quotation marks (" ") in some cases. See "CS+ Integrated Development Environment User’s Manual: Debug Tool" for details. |