This function clears the mapping settings.
[Specification format]
[Argument(s)]
None
[Return value]
If the memory map was cleared successfully: True
If there was an error when clearing the memory map: False
[Detailed description]
- | This function clears the mapping settings. |
[Example of use]
>>>debugger.Map.Clear()
True
>>>
|