debugger.Trace.Enable


This function enables a conditional trace.

[Specification format]

debugger.Trace.Enable(traceNumber = "")

[Argument(s)]

Argument

Description

traceNumber

Specify the trace event number to enable.

[Return value]

If a trace setting was enabled successfully: True

If there was an error when enabling a trace setting: False

[Detailed description]

-

This function enables the timer of the trace event specified by traceNumber.

-

If traceNumber is not specified, then traces of all trace event numbers will be enabled.

[Example of use]

>>>debugger.Trace.enable(1)
True
>>>