debugger.Interrupt.DeleteTimer


This function deletes the timer interrupt setting. [RH850 Simulator]

Remark

This function provides the same function as debugger.XRunBreak.Delete.

[Specification format]

debugger.Interrupt.DeleteTimer()

[Argument(s)]

None

[Return value]

If the timer interrupt setting was deleted successfully: True

If there was an error when deleting the timer interrupt setting: False

[Detailed description]

-

This function deletes the timer interrupt setting.

[Example of use]

>>>debugger.Interrupt.ReferTimer()
None
>>>debugger.Interrupt.SetTimer(1, TimeType.S, True)
True
>>>debugger.Interrupt.ReferTimer()
1Second Periodic
>>>debugger.Interrupt.DeleteTimer()
True
>>>debugger.Interrupt.ReferTimer()
None