debugger.Breakpoint.Enable


This function enables a break point setting.

[Specification format]

debugger.Breakpoint.Enable(breakNumber = "")

[Argument(s)]

Argument

Description

breakNumber

Specify the break event number to enable.

[Return value]

If a break point setting was enabled successfully: True

If there was an error when enabling a break point setting: False

[Detailed description]

-

This function enables the break event specified by breakNumber.

-

If breakNumber is not specified, then breaks of all break event numbers will be enabled.

[Example of use]

>>>debugger.Breakpoint.Enable(1)
True
>>>debugger.Breakpoint.Disable(1)
True
>>>debugger.Breakpoint.Delete(1)
True
>>>