debugger.Breakpoint.Set


This function configures a break point.

[Specification format]

debugger.Breakpoint.Set(BreakCondition)

[Argument(s)]

Argument

Description

BreakCondition

Specify a break condition.

See the BreakCondition property for details about creating break conditions.

[Return value]

Set break event number (numerical value)

[Detailed description]

-

This function sets a break point according to the specifications in BreakCondition.

-

break-name is "PythonBreakxxxx" (xxxx: 4-digit number).

[Example of use]

>>>Condition = BreakCondition()
>>>Condition.Address = "main"
>>>breakNumber = debugger.Breakpoint.Set(Condition)
1
>>>print breakNumber
1
>>>debugger.Breakpoint.Information()
   1 PythonBreak0001 Enable  0x000002dc