debugger.XCoverage.Clear


This function clears the coverage memory. [IECUBE][IECUBE2][Simulator]

[Specification format]

debugger.XCoverage.Clear()

[Argument(s)]

None

[Return value]

If the coverage memory was cleared successfully: True

If there was an error when clearing the coverage memory: False

[Detailed description]

-

This function clears the coverage memory.

[Example of use]

>>>debugger.XCoverageClear()
True
>>>