debugger.Performance.Get


This function references the result of performance measurement. [RH850][E1/E2/E20/Full-spec emulator]

[Specification format]

debugger.Performance.Get()

[Argument(s)]

None

[Return value]

List of performance measurement information (see the PerformanceInfo class for detail)

[Detailed description]

-

Performance measurement information is shown by the following format.

[performance-measurement-event-number] [count] [performance-measurement-mode] [performance-measurement-item]

[Example of use]

>>>pf = debugger.Performance.Get()
1 2030 MaxCount AllFetchCall
2 3000 MinCount AllFetchBranch
>>>print pf[0].Count
2030
>>>print pf[0].Mode
PerformanceMode.MaxCount
>>>