debugger.Memory.Copy


This function copies the memory.

[Specification format]

debugger.Memory.Copy(address1, address2, address3)

[Argument(s)]

Argument

Description

address1

Specify the start address to copy from.

address2

Specify the end address to copy from.

address3

Specify the address to copy to.

[Return value]

If the memory was copied successfully: True

If there was an error when copying the memory: False

[Detailed description]

-

This function copies the memory from address1 to address2 into address3.

[Example of use]

>>>debugger.Memory.Copy(0x1000, 0x2000, 0x3000)
True
>>>