Everything
 

Detailed Settings of Timer Measurement dialog box [Full-spec emulator][E1][E20]


This dialog box is used to display and change the detailed information on the timer event selected on the Events panel. Note that you cannot edit the address value of the timer event in this dialog box. If you need to edit the address value, first delete the timer event and then create a new one. For details on timer event setting, see "2.15 Measure Execution Time of Programs".

Figure A.48

Detailed Settings of Timer Measurement Dialog Box [Full-spec emulator][E1][E20]

 

This section describes the following.

[How to open]

-

On the Events panel, move the caret to the timer event of which you wish to change the detailed information, then select [Edit Condition ...] from the context menu.

[Description of each area]

(1)

Detailed information display/change area

In this area, detailed information on the timer event selected in the Events panel is displayed by category in the list. Also, you can directly change its settings.

(2)

Property description area

In this area, brief description of the categories and properties selected in the detailed information display/change area is displayed.

[Toolbar]

 

Displays categories in the detailed information display/change area.

 

Hides categories in the detailed information display/change area and rearranges only property items in the ascending order.

[Description of each category]

(1)

[Measurement Setting]

You can display and modify the detailed settings on timer measurement.

Measurement item

Specify the measurement item.

Default

The current set value

Modifying

Select from the drop-down list.

Available values

One of the following as selected from the drop-down list.

Total Count, Max Count, Min Count, Pass Count

[Function buttons]

Button

Function

OK

Applies the detailed settings specified in the dialog box to the timer event and closes this dialog box.

Cancel

Nullifies settings and closes this dialog box.

Help

Displays the help for this dialog box.