Everything
 

Flash Options Setting dialog box


This dialog box is used to configure options for the flash memory incorporated in the microcontroller.

Caution 1.

[Full-spec emulator][E1][E20]
This dialog box appears only when connecting to the debug tool.
[Simulator]
This dialog box appears only when disconnecting from the debug tool.

Caution 2.

[Full-spec emulator][E1][E20]
CPU reset may be generated automatically when you click the [Write] button after changing the configuration of this dialog box.

Figure A.28

Flash Options Setting Dialog Box [Full-spec emulator][E1][E20]

Figure A.29

Flash Options Setting Dialog Box [Simulator]

 

This section describes the following.

[How to open]

-

On the [Flash Options Settings] tab tab of the Property panel, click the [...] button displayed by selecting the [Flash options] property in the [Flash Options] category.

[Description of each area]

(1)

[Flash option property] area

(a)

[Option Bytes Setting]

You can configure the option bytes for the flash memory.

OPBT0 - 15

Specify the option bytes.

Default

The initial value stored in the device file.

Modifying

Directly enter from the keyboard.

Available values

0x0 to 0xFFFFFFFF in hexadecimal number

Caution

The number of option bytes (OPB0 - 15) to be displayed differs with the selected microcontroller (the bytes for some numbers might actually be unused).

[Function buttons]

Button

Function

Read

[Full-spec emulator][E1][E20]

Reads the values currently specified in the debug tool, and reflects them in this dialog box.

Write

[Full-spec emulator][E1][E20]

Writes the currently set values in this dialog box to the debug tool, and reflects them in the project. Then, closes this dialog box.

Close

Specifies the currently set values in this dialog box to the project and closes this dialog box.

Cancel

Closes this dialog box without setting.

Help

Displays the help for this dialog box.