Everything
 

Select Debug target dialog box


This dialog box is used to set the debugging.

Figure A.22

Select Debug target Dialog Box

 

The following items are explained here.

[How to open]

-

On the [Connect Settings] tab of the Property panel, click the [...] button displayed by selecting one of the values of the [Debug target] property in the [Multi-core] category.

[Description of each area]

(1)

Area with a list of contexts for debugging

This area displays a list of contexts for debugging.

When a checkbox is selected, the selected context is handled as a target for debugging.

The checkboxes are selected by default.

[Function buttons]

Button

Function

OK

Completes the settings of contexts for debugging and closes this dialog box.

Cancel

Cancels the modification of contexts for debugging and closes this dialog box.

Help

Displays the help of this dialog box.