Everything
 

Select SPID filter dialog box


This dialog box is used to set the SPID filter.

Figure A.24

Select SPID filter Dialog Box

 

The following items are explained here.

[How to open]

-

On the [Debug Tool Settings] tab of the Property panel, click the [...] button displayed by selecting one of the values of the [SPID filter] property in the [Trace] category.

[Description of each area]

(1)

Area with a list of SPIDs

This area displays a list of SPIDs.

When a checkbox is selected, trace information for the SPID with the given number is collected. The checkboxes are selected by default.

(2)

Area for the [Select All/Release All] checkbox

(a)

Select All/Release All checkbox

All checkboxes in the area with the list of SPIDs are selected or deselected.

Selecting this checkbox selects all checkboxes in the area with the list of SPIDs.

Deselecting this checkbox deselects all checkboxes in the area with the list of SPIDs.

[Function buttons]

Button

Function

OK

Completes the settings of the SPID filter and closes this dialog box.

Cancel

Cancels the modification of the SPID filter and closes this dialog box.

Help

Displays the help of this dialog box.