3.2.48 12-bit D/A converter

Below is a list of API functions output by the Code Generator for 12-bit D/A converter use.

Table 3.48

API Functions: [12-bit D/A Converter]

API Function Name

Function

R_12DA_Create

Performs initialization necessary to control the 12-bit D/A converter.

R_12DA_Create_UserInit

Performs user-defined initialization relating to the 12-bit D/A converter.

R_12DAn_Start

Starts D/A conversion.

R_12DAn_Stop

Ends D/A conversion.

R_12DA_Set_PowerOff

Halts the clock supplied to the 12-bit D/A converter.

R_12DAn_Set_ConversionValue

Sets the analog voltage output to the ANOn pin.