3.2.44 Operational amplifier

Below is a list of API functions output by the Code Generator for Operational Amplifier use.

Table 3.44

API Functions: [Operational amplifier]

API Function Name

Function

R_OPAMP_Create

Performs initialization necessary to control the operational amplifier.

R_OPAMP_Create_UserInit

Performs user-defined initialization relatede to the operational amplifier.

R_OPAMP_Set_ReferenceCurcuitOn

Enables operational amplifier reference current circuit.

R_OPAMP_Set_ReferenceCircuitOff

Disables operational amplifier reference current circuit.

R_OPAMPn_Start

Starts operational amplifier of unit n.

R_OPAMPn_Stop

Stops operational amplifier of unit n.

R_OPAMPn_Set_PrechargeOn

Starts precharging of the external capacitor of the operational amplifier n.

R_OPAMPn_Set_PrechargeOff

Performs user-defined initialization relatede to the operational amplifier.