3.2.36 Data transfer controller

Below is a list of API functions output by the Code Generator for Data transfer controller use.

Table 3.36

API Functions: [Data transfer controller]

API Function Name

Function

R_DTC_Create

Performs initialization necessary to control the Data transfer controller.

R_DTC_Create_UserInit

Performs user-defined initialization relating to the Data transfer controller.

R_DTCn_Start

Enables operation of the Data transfer controller.

R_DTCn_Stop

Disables operation of the Data transfer controller.

R_DTC_Set_PowerOff

Halts the clock supplied to the Data transfer controller.