3.2.25 D/A converter

Below is a list of API functions output by the Code Generator for D/A converter use.

Table 3.25

API Functions: [D/A Converter]

API Function Name

Function

R_DAC_Create

Performs initialization necessary to control the D/A converter.

R_DAC_Create_UserInit

Performs user-defined initialization relating to the D/A converter.

R_DACn_Start

Starts D/A conversion.

R_DACn_Stop

Ends D/A conversion.

R_DAC_Set_PowerOff

Halts the clock supplied to the D/A converter.

R_DACn_Set_ConversionValue

Sets the analog voltage output to the ANOn pin.

R_DAC_Change_OutputVoltage_8bit

Changes the output voltage of D/A converter.(8bit mode)

R_DAC_Change_OutputVoltage

Changes the output voltage of D/A converter.(12bit mode)

R_DACn_Create

Performs initialization necessary to control the D/A converter.

R_DAC_Reset

Reset the D/A converter.