3.2.34 Sound generator

Below is a list of API functions output by the Code Generator for sound generator use.

Table 3.34

API Functions: [Sound Generator]

API Function Name

Function

R_SG_Create

Performs initialization necessary to control the sound generator.

R_SG_Create_UserInit

Performs user-defined initialization relating to the sound generator.

r_sg_interrupt

Performs processing in response to the threshold value detection of the logarithmic decrement interrupt INTSG.

R_SG_Start

Enables operation of sound generator.

R_SG_Stop

Disables operation of sound generator.