Renesas Electronics
Below is a list of API functions output by the Code Generator for Operational Amplifier and Analog switch use.
Table 3.49
API Functions: [Operational amplifier and Analog switch]
API Function Name
Function
R_AMPANSW_Create
Performs initialization necessary to control the Operational amplifier and Analog switch.
R_AMPANSW_Create_UserInit
Performs user-defined initialization relating to the Operational amplifier and Analog switch.
R_OPAMPm_Set_ReferenceCurcuitOn
Enables operational amplifier reference current circuit.
R_OPAMPm_Set_ReferenceCircuitOff
Disables operational amplifier reference current circuit.
R_OPAMPm_Start
Starts operational amplifier of unit m.
R_OPAMPm_Stop
Stops operational amplifier of unit m.
R_ANSW_ChargePumpm_On
Enables analog switch of unit m.
R_ANSW_ChargePumpm_Off
Disables analog switch of unit m.