Renesas Electronics
Below is a list of API functions output by the Code Generator for SPI interface use.
Table 3.43
API Functions: [SPI Interface]
API Function Name
Function
R_SAIC_Create
Performs initialization necessary to control the SPI interface.
R_SAIC_Create_UserInit
Performs user-defined initialization relating to the SPI interface.
R_SAIC_Write
Starts SPI data transmission.
R_SAIC_Read
Starts SPI data reception.