Renesas Electronics
Below is a list of API functions output by the Code Generator for timer RG use.
Table 3.8
API Functions: [Timer RG]
API Function Name
Function
R_TMR_RG0_Create
Performs initialization necessary to control the 16-bit timer RG0.
R_TMR_RG0_Create_UserInit
Performs user-defined initialization relating to the 16-bit timer RG0.
r_tmr_rg0_interrupt
Performs processing in response to the timer interrupt.
R_TMR_RG0_Start
Starts the count for 16-bit timer RG0.
R_TMR_RG0_Stop
Ends the count for 16-bit timer RG0.
R_TMR_RG0_Set_PowerOff
Halts the clock supplied to the 16-bit timer RG0.
R_TMR_RG0_Get_PulseWidth
Reads the pulse width of the 16-bit timer RG0.