11. Renesas Skills for AI Coding Assistants
Renesas Skills is a collection of skills that help AI coding assistants work better with the projects in VS Code. The skills follow the shared Agent Skills specification, which makes them agent-agnostic. They work with Claude Code, GitHub Copilot, Cursor and many other agents supported by skills.sh.
11.1. Available Skills
Skill |
Description |
|---|---|
|
Generates and modifies |
11.2. Requirements
Node.js version 22.20.0 or later, which is required to run
npx. It can be downloaded from the Node.js website.Access to the npm registry
11.3. Installation
The skills are installed with the skills.sh CLI. The most common installation commands are given below. Further options are described in the README.md file of the repository.
To install the skills for the current project, run the following command from the project root:
npx skills add renesas/renesas-skills
To install the skills once so that they are available across all projects, run the following command:
npx skills add renesas/renesas-skills -g
By default, the skills are installed as symbolic links. On Windows, if the creation of symbolic links fails, add the --copy option to install file copies instead.
Important
The editor or agent must be restarted after the installation, so that the new skills are loaded.
11.4. Further Information
The README.md file in the renesas-skills repository provides further details, including:
The device families and debuggers covered by each skill
The supported agents and their installation paths
The installation options for specific agents
The commands for listing, updating and removing skills
Troubleshooting information for skills that are not loaded by an agent