BCnd

Relative conditional branch

BCnd

Branch Conditionally


[Syntax]

BCnd(.length) src

 

[Operation]

if ( Cnd )

PC = PC + src;

 

[Function]

-

This instruction logically ANDs dest and src and stores the result in dest.

-

If dest is A0 or A1 and the selected size specifier (.size) is (.B), src is zero-expanded to perform calculation in 16. If src is A0 or A1, operation is performed on the eight low-order bits of A0 or A1.

BCnd

Condition

Expression

BGEU,

BC

C == 1

Equal to or greater than/C flag is 1

<=

BEQ,

BZ

Z == 1

Equal to/Z flag is 1

=

BGTU

(C & ~Z) == 1

Greater than

<

BPZ

S == 0

Positive or zero

> 0

BGE

(S ^ O) == 0

Equal to or greater than as signed integer

<=

BGT

((S ^ O) |Z) == 0

Greater than as signed integer

<

BO

O == 1

O flag is 1

 

BLTU,

BNC

C == 0

Less than/C flag is 0

<=

BNE,

BNZ

Z == 0

Not equal to/Z flag is 0

 

BLEU

(C & ~Z) == 0

Equal to or less than

 

BN

S == 1

Negative

0>

BLE

((S ^ O) |Z) == 1

Equal to or less than as signed integer

>=

BLT

(S ^ O) == 1

Less than as signed integer

>

BNO

O == 0

O flag is 0

 

 

[Instruction Format]

Syntax

Processng Size

Operand

Code Size

(Byte)

src

Range of pcdsp

BEQ.S src

S

pcdsp:3

3 ≤ pcdsp ≤ 10

1

BNE.S src

S

pcdsp:3

3 ≤ pcdsp ≤ 10

1

BCnd.B src

B

pcdsp:8

-128 ≤ pcdsp ≤ 127

2

BEQ.W src

W

pcdsp:16

-32768 ≤ pcdsp ≤ 32767

3

BNE.W src

W

pcdsp:16

-32768 ≤ pcdsp ≤ 32767

3

 

[Flag Change]

This instruction does not affect the states of flags.

 

[Description Example]

BC label1

BC.B label2

Note

For the RX Family assembler manufactured by Renesas Technology Corp., enter a destination address specified by a label or an effective address as the displacement value (pcdsp:3, pcdsp:8, pcdsp:16). The value of the specified address minus the address where the instruction is allocated will be stored in the pcdsp section of the instruction.

BC label

BC 1000h