* SP is always decremented by 4 even when the size specifier (.size) is .B or .W. The higher-order 24 and 16 bits in the respective cases (.B and .W) are undefined.  | 
When src is in register and the size specifier for the PUSH instruction is .B or .W, the byte or word of data from the LSB in the register are saved respectively.  | 
The transfer to the stack is processed in longwords. When the size specifier is .B or .W, the higher-order 24 or 16 bits are undefined respectively.  |