ITOF

Integer to floating-point conversion

ITOF

Integer TO Floating-point


[Syntax]

ITOF src, dest

 

[Operation]

dest = ( float ) src;

 

[Function]

-

This instruction converts the signed longword (32-bit) integer stored in src into a single-precision floating-point number and places the result in dest. Rounding of the result is in accord with the setting of the RM[1:0] bits in the FPSW. 00000000h is handled as +0 regardless of the rounding mode.

 

[Instruction Format]

Syntax

Processng Size

Operand

Code Size

(Byte)

src

dest

ITOF src, dest

L

Rs

Rd

3

L

[Rs].memex

Rd

3 (memex == UB)

4 (memex != UB)

L

dsp:8[Rs].memex

Rd

4 (memex == UB)

5 (memex != UB)

L

dsp:16[Rs].memex

Rd

5 (memex == UB)

6 (memex != UB)

[Flag Change]

Flag

C

Z

S

O

CV

CO

CZ

CU

CX

CE

FV

FO

FZ

FU

FX

Change

–

 

 

–

 

 

 

 

 

 

–

–

–

–

 

Conditions

Z : The flag is set if the result of the operation is +0; otherwise it is cleared.

S : The flag is set if the sign bit (bit 31) of the result of the operation is 1; otherwise it is cleared.

CV : The value of the flag is always 0.

CO : The value of the flag is always 0.

CZ : The value of the flag is always 0.

CU : The value of the flag is always 0.

CX : The flag is set if an inexact exception is generated; otherwise it is cleared.

CE : The value of the flag is always 0.

FX : The flag is set if an inexact exception is generated; otherwise it does not change.

Note

The FX flag does not change if the exception enable bit EX is 1. The S and Z flags do not change when an exception is generated.

 

[Description Example]

ITOF R1, R2

ITOF [R1], R2

ITOF 16[R1].L, R2