|
MVFACLO
|
Move the lower-order longword from the accumulator
[V2.01.00 or later]
|
MVFACLO
|
|
MoVe From ACcumulator LOw-order longword
|
[Syntax]
MVFACLO src, Asrc, dest
[Operation]
signed 72bit tmp;
tmp = (signed 72bit) Asrc << src;
dest = (signed long) tmp;
[Function]
- | The MVFACLO instruction is executed according to the following procedures. |
Processing 1:
The value of the accumulator is shifted to the left by zero to two bits as specified by src.
Processing 2:
This instruction moves the contents of bits 31 to 0 of the accumulator (ACC0 or ACC1) to dest.
- | You can assemble assembly-language code that includes this instruction if you have specified the assembler option -isa with selection of the instruction set of the RXv2 or a later version. |
[Instruction Format]
|
|
|
|
|
|
|
|
|
MVFACLO src, Asrc, dest
|
#IMM:2
(IMM:2 = 0 to 2)
|
A0, A1
|
Rd
|
|
Note | Specify A0 (ACC0) or A1 (ACC1) as Asrc. |
[Flag Change]
This instruction does not affect the states of flags.
[Description Example]
MVFACLO #1, A1, R1