EXTB is also specifiable as dest if you have specified the assembler option -isa with selection of the instruction set of the RXv2 or a later version. [V2.01.00 or later]  | 
In user mode, writing to the ISP, INTB, EXTB, BPC, BPSW, and FINTV, and the IPL[3:0], PM, U, and I bits in the PSW is ignored. In supervisor mode, writing to the PM bit in the PSW is ignored.  | 
* Selectable dest: Registers ISP, USP, INTB, EXTB, PSW, BPC, BPSW, FINTV, and FPSW  |