|
Multiply-Accumulate the lower-order word and higher-order word [V2.01.00 or later] |
||
tmp2 = (signed short) (src2 >> 16);
tmp3 = (signed long) tmp1 * (signed long) tmp2;
This instruction multiplies the lower-order 16 bits of src by the higher-order 16 bits of src2, and adds the result to the value in the accumulator (ACC0 or ACC1). The addition is performed with the least significant bit of the result of multiplication corresponding to bit 16 of ACC. The result of addition is stored in ACC. The lower-order 16 bits of src and the higher-order 16 bits of src2 are treated as signed integers. You can assemble assembly-language code that includes this instruction if you have specified the assembler option -isa with selection of the instruction set of the RXv2 or a later version.