RSTR

Restoring the values of registers [V3.00.00 or later]

RSTR


[Syntax]

RSTR src

 

[Operation]

{ R1, R2, R3, R4, R5, R6, R7, R8, R9, R10, R11, R12, R13, R14, R15, USP, FPSW, ACC0, ACC1 } = register_bank(src);

 

[Function]

-

The values are restored from the register bank to registers of the CPU (R1 to R15, USP, FPSW, ACC0, and ACC1).

-

The bank number of the source for restoration is specified by src.

-

This instruction is privileged. Attempting to execute it in user mode leads to a privileged instruction exception.

-

Regarding whether or not a device has register bank and, if so, its capacity and the actual range of bank numbers (determined by the capacity of the memory provided for register banks) that is available, refer to the hardware manuals for the respective products.

-

When a bank number that does not exist is specified, the operation is not defined.

-

You can assemble assembly-language code that includes this instruction if you have specified the assembler option -isa with selection of the instruction set of the RXv3 or a later version.

 

[Instruction Format]

Syntax

Processng Size

Operand

Code Size

(Byte)

src

RSTR src

−

#UIMM:8

4

−

Rs

4

 

[Flag Change]

This instruction does not affect the states of flags.

 

[Description Example]

RSTR #5

RSTR R1