| 
 MVFACGU 
 | 
 
Move the guard longword from the accumulator 
[V2.01.00 or later] 
 | 
 
MVFACGU 
 | 
| 
 
MoVe From ACcumulator GUard longwor 
 | 
[Syntax]	
MVFACGU    src, Asrc, dest
 
[Operation]
signed 72bit tmp;
tmp = (signed 72bit) Asrc << src;
dest = (signed long) (tmp >> 64);
 
[Function]
-  | The MVFACGU instruction is executed according to the following procedures.  | 
 
Processing 1:
The value of the accumulator is shifted to the left by zero to two bits as specified by src.
Processing 2:
This instruction moves the higher-order 32 bits of the accumulator (ACC0 or ACC1) to dest.
-  | You can assemble assembly-language code that includes this instruction if you have specified the assembler option -isa with selection of the instruction set of the RXv2 or a later version.  | 
 
 
[Instruction Format]
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 
MVFACGU    src, Asrc, dest 
 | 
 
#IMM:2 
(IMM:2 = 0 to 2) 
 | 
 
A0, A1 
 | 
 
Rd 
 | 
 | 
 
Note  | Specify A0 (ACC0) or A1 (ACC1) as Asrc.  | 
 
 
[Flag Change]
This instruction does not affect the states of flags.
 
[Description Example]
MVFACGU    #1, A1, R1