Everything
 

Progress Status dialog box


This dialog box is used to display how the process has been progressed when the time consuming process is taken place.

This dialog box automatically closes when the process in progress is done.

Figure A.32

Progress Status Dialog Box

 

The following items are explained here.

[How to open]

-

The dialog box automatically opens when a message is output while the time consuming process is in progress.

[Description of each area]

(1)

Message display area

Displays the message output while process is in progress (edit not allowed).

(2)

Progress bar

The progress bar shows the current progress of the process in progress with the bar length.

When the process is 100% done (the bar gets to the right end), this dialog box automatically closed.

[Function buttons]

Button

Function

Cancel

Cancels the process in progress and closes this dialog box.

Note that if the process termination is impossible, this button is disabled.