24-bit DS A/D converter
Below is a list of API functions output by the Code Generator for 24-bit ΔΣ A/D converter use.
Table 3.25 API Functions: [224-bit ΔΣ A/D Converter]
|
API Function Name |
Function |
|
Performs initialization necessary to control the 24-bit ΔΣ A/D converter. | |
|
Performs user-defined initialization relating to the 24-bit ΔΣ A/D converter. | |
|
Performs processing in response to the ΔΣ A/D conversion end interrupt INTDSAD. | |
|
Performs processing in response to the zero-cross detection interrupt INTDSADZCn. | |
|
Enables operation of 24-bit ΔΣ A/D converter. | |
|
Disables operation of 24-bit ΔΣ A/D converter. | |
|
Starts A/D conversion. | |
|
Ends A/D conversion. | |
|
Reset the 24-bit ΔΣ A/D converter. | |
|
Performs electric charge reset for the 24-bit ΔΣ A/D converter. | |
|
Reads the results of A/D conversion (24 bits). | |
|
Reads the results of A/D conversion (16 bits; most significant 16 bits of 24-bit resolution). |