Operational amplifier and Analog switch
Below is a list of API functions output by the Code Generator for Operational Amplifier and Analog switch use.
Table 3.51 API Functions: [Operational amplifier and Analog switch]
API Function Name |
Function |
Performs initialization necessary to control the Operational amplifier and Analog switch. | |
Performs user-defined initialization relating to the Operational amplifier and Analog switch. | |
Enables operational amplifier reference current circuit. | |
Disables operational amplifier reference current circuit. | |
Starts operational amplifier of unit m. | |
Stops operational amplifier of unit m. | |
Enables analog switch of unit m. | |
Disables analog switch of unit m. |