Configurable amplifier
Below is a list of API functions output by the Code Generator for configurable amplifier use.
Table 3.23 API Functions: [Configurable amplifier]
API Function Name |
Function |
Performs initialization necessary to control the configurable amplifier. | |
Performs user-defined initialization relating to the configurable amplifier. | |
Turns on the power of the configurable amplifier(AMPn). | |
Turns off the power of the configurable amplifier(AMPn). | |
Halts the clock supplied to the configurable amplifier. |