Oscillation stop detector
Below is a list of API functions output by the Code Generator for oscillation stop detector use.
Table 3.44 API Functions: [Oscillation Stop Detector]
API Function Name |
Function |
Performs initialization necessary to control the oscillation stop detector. | |
Performs user-defined initialization relating to the oscillation stop detector. | |
Performs processing in response to the oscillation stop detection interrupt INTOSDC. | |
Enables operation of oscillation stop detector. | |
Disables operation of oscillation stop detector. | |
Halts the clock supplied to the oscillation stop detector. | |
Reset the oscillation stop detector. |