Sound generator
Below is a list of API functions output by the Code Generator for sound generator use.
Table 3.36 API Functions: [Sound Generator]
API Function Name |
Function |
Performs initialization necessary to control the sound generator. | |
Performs user-defined initialization relating to the sound generator. | |
Performs processing in response to the threshold value detection of the logarithmic decrement interrupt INTSG. | |
Enables operation of sound generator. | |
Disables operation of sound generator. |