Everything

Timer RX

Below is a list of API functions output by the Code Generator for timer RX use.

 

Table 3.9   API Functions: [Timer RX]

API Function Name

Function

R_TMRX_Create

Performs initialization necessary to control the 16-bit timer RX.

R_TMRX_Create_UserInit

Performs user-defined initialization relating to the 16-bit timer RX.

r_tmrx_interrupt

Performs processing in response to the timer interrupt.

R_TMRX_Start

Starts the count for 16-bit timer RX.

R_TMRX_Stop

Ends the count for 16-bit timer RX.

R_TMRX_Set_PowerOff

Halts the clock supplied to the 16-bit timer RX.

R_TMRX_Get_BufferValue

Reads the buffer value of TRX resister(16-bit timer RX).